iMX8M plus - M7 trigger watchdog and A53 halt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M plus - M7 trigger watchdog and A53 halt

1,688 Views
sophiehu
Contributor III

Hi NXP,

There are A53 and M7 in iMX8M plus EVK and I wish I can establish a data link between A53 and M7 to keep them sync data (maybe just simple echo or ping-pong). Once the data sync is missing over timeout time, I can make M7 trigger watchdog to reset A53 and itself.

I download M7 SDK from https://mcuxpresso.nxp.com/en/select and verify the watchdog example.
There are some problems:
1. M7 can trigger watchdog to reset itself, but A53 halt when M7 trigger watchdog
2. Once A53 halt, M7 trigger watchdog again, and M7 halt
3. M7 can not free run. There's no debug message output by M7.

To test and verify:
M7: wdog example (SDK_2_10_0_EVK-MIMX8MP\boards\evkmimx8mp\driver_examples\wdog)
A53: run a simple script to show the date and time every two seconds to confirm if it is working

1. M7 can trigger the first watchdog to reset itself, but A53 halt when M7 triggered the first watchdog.
Then M7 triggers the second watchdog and halt.
01.jpg

2. Modify watchdog example to ignore the first trigger software reset testing.
No matter it starts from power on reset or software reset, it will run watchdog timeout reset testing

sophiehu_1-1629958946423.png
When M7 watchdog timeout and trigger reset, A53 still halt

sophiehu_2-1629959002907.jpeg

3. Remove segger j-link debugger, turn off power and turn on to let M7 free run.
There's no debug message output from M7.
I test hello_world example (\SDK_2_10_0_EVK-MIMX8MP\boards\evkmimx8mp\demo_apps\hello_world), and there's no debug message output either.
I also download and debug by IAR and it is OK, but there's no debug message output when free run either.

Sophie

0 Kudos
6 Replies

1,133 Views
sonfly
Contributor I

M7 can trigger watchdog to reset itself, but A53 halt when M7 trigger watchdog

I'm hitting the same issue on imx8mp evk (MIMX8ML8), even though WDOG3_RST_OPTION and WDOT3_RST_OPTION_M7 of SRC_M7RCR (3039_000C) have been set to 0. We need the wdog to reset the M core only. Please note that this works on imx8mm evk (MIMX8MM6).

I have tried all 4 combinations of 00,01,10,11, none of them fixes the issue.

sonfly_0-1667162028319.png

Could anyone provide some advice?

0 Kudos

1,671 Views
sophiehu
Contributor III

Hi Igor,

BTW, about question3, how to make M7 free run? (without j-link debugger)
I cannot make M7 do anything if it can not free run.

Sophie

0 Kudos

1,671 Views
sophiehu
Contributor III

Hi Igor,

In IMX8MPRM.pdf (i.MX 8M Plus Applications Processor Reference Manual)
Chapter 6.6 Watchdog Timer (WDOG)
I don't quite understand this description.
Will A53 custom timeout watchdog trigger WDOG_B to reset pmic to reset both A53 and M7?
User can custom watchdog timer 0.5 ~ 128 secs, which will trigger WDOG_RESET_B_DEB.
What happen when WDOG_RESET_B_DEB triggered?
What reset fixed 16 secs power down counter to prevent it trigger WDOG_B to reset pmic?

sophiehu_0-1630027606202.png


Can M7 trigger WDOG_B, too?
If yes, M7 can do what I want it to do.
Besides, is this resetting flow correct?
M7 watchdog timeout -> A53 halt -> A53 watchdog timeout -> reset pmic -> reset both A53 and M7.

Sophie

0 Kudos

1,667 Views
igorpadykov
NXP Employee
NXP Employee

>Will A53 custom timeout watchdog trigger WDOG_B to reset pmic to reset both A53 and M7?

 

yes, please look at first answer.

 

Best regards
igor

0 Kudos

1,664 Views
sophiehu
Contributor III

Can M7 trigger WDOG_B, too?

 

0 Kudos

1,679 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sophie

 

I am afraid such A53 reset is not supported in BSPs, supported case with signal

WDOG_B (CPU WDOG_B Reset) on i.MX8M PLus LPDDR4 EVK schematic, SPF-46368 p.11

resetting pmic PCA9450CHN (U6C).

 

Best regards
igor

0 Kudos