iMX6ULL TDM with MAX98357A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6ULL TDM with MAX98357A

2,658 次查看
rogersclark
Contributor II

How do the iMX6ULL ESAI pins map to I2S pins?

I want to connect eight MAX98357A PCM input class D power amps to the ESAI interface.

标签 (1)
标记 (4)
7 回复数

2,185 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rogers

please check imx6ull-14x14-ddr3-arm2-cs42888.dts

linux-imx.git - i.MX Linux Kernel 

linux-imx.git - i.MX Linux Kernel 

AM1848 ESAI

http://www.nxp.com/docs/en/application-note/AN1848.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,185 次查看
rogersclark
Contributor II

Igor,

Thank you for your response, but I've been studying that application note(AN1848) for a few days.

I still don't understand how the iMX6ULL ESAI pins map to I2S pins.

AN1848 Table 1-2 describes the following ESAI pins:

SCKR, FSR, HCKR, SCKT, FST, HCKT, SDO5/SDI0, SDO4/SDI1, SDO3/SDI2, SDO1, SDO0.

The iMX6ULL datasheet doesn't reference the names of the ESAI pins.

The Pins for i.MX software names the following ESAI pins:

RX_CLK, RX_FS, RX_HF_CLK, TX0, TX1, TX2_RX3, TX3_RX2, TX4_RX1, TX5_RX0, TX_CLK, TX_FS, HF_CLK

I2S is commonly: DataOut, DataIn, BitCLK, FrameCLK, MasterCLK

The MAX98357 only uses: BitCLK, FrameCLK, and DataIN

On the iMX6ULL ESAI interface, which pins should be connected to BitCLK, FrameCLK, and DataIN?

Best regards,

Rogers

0 项奖励
回复

2,185 次查看
rogersclark
Contributor II

Igor,

I may have just figured it out:

BitCLK = HF_CLK

FrameCLK = TX_FS

DataIN = TX0

Is that correct?

Best regards,

Rogers

0 项奖励
回复

2,185 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rogers

from linux-imx.git - i.MX Linux Kernel 

          pinctrl_esai: esaigrp {                fsl,pins = <                     MX6UL_PAD_CSI_DATA00__ESAI_TX_HF_CLK     0x1b0b0                     MX6UL_PAD_CSI_DATA01__ESAI_RX_HF_CLK     0x1b0b0                     MX6UL_PAD_CSI_DATA04__ESAI_TX_FS         0x1b0b0                     MX6UL_PAD_CSI_DATA05__ESAI_TX_CLK        0x1b0b0                     MX6UL_PAD_CSI_DATA07__ESAI_T0            0x1b0b0                     MX6UL_PAD_CSI_HSYNC__ESAI_TX1            0x1b0b0                     MX6UL_PAD_CSI_PIXCLK__ESAI_TX2_RX3       0x1b0b0                     MX6UL_PAD_CSI_MCLK__ESAI_TX3_RX2         0x1b0b0                     MX6UL_PAD_CSI_DATA02__ESAI_RX_FS         0x1b0b0                     MX6UL_PAD_CSI_DATA03__ESAI_RX_CLK        0x1b0b0                     MX6UL_PAD_CSI_DATA06__ESAI_TX5_RX0       0x1b0b0                     MX6UL_PAD_CSI_VSYNC__ESAI_TX4_RX1        0x1b0b0                >;           };

also please check sect.4.3 I2S, LEFT-JUSTIFIED, AND EIAJ (RIGHT JUSTIFIED) FORMATS AN1848

Best regards
igor
0 项奖励
回复

2,185 次查看
rogersclark
Contributor II

Igor,

I appreciate your help, but I'm a hardware engineer trying to figure out which pins to connect the on iMX6 to the MAX98357. I do not understand that code.

My problem is the naming convention from the app note doesn't match the pin names found elsewhere.

I think frame sync is D4 and the data outs are D1, F3, E5, F5, F2, D2. But, which is the bit clock? Pin D3 or E4?

Best regards,

Rogers

0 项奖励
回复

2,185 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rogers

please look at Table 3. ESAI PINMUX AN5350 i.MX 6ULL Migration Guide 

http://www.nxp.com/docs/en/application-note/AN5350.pdf 

Best regards
igor

0 项奖励
回复

2,185 次查看
rogersclark
Contributor II

Igor,

Thanks for your help.

After I test my board, I'll update this thread.

Best regards,

Rogers

0 项奖励
回复