Hi,
I am using iMX6UL in my design with JEDEC/MMC version 4.51 compliant eMMC MTFC4GACAAAM-1M WT. The eMMC part i am planning to use is not recommended for new design.
So I want to move to new part which is MMC version 5.0 compliant eMMC MTFC4GACAJCN-1M WT.
As per datasheet iMX6UL supports MMC version 4.4/4.5.
Can i use ver 5.0 compliant eMMC MTFC4GACAJCN-1M WT with iMX6UL processor.?
Seeking for help.
Thank you.
Original Attachment has been moved to: Micron_eMMC.zip
Hello Ritesh Patel,
You should be able to use the eMMC 5.0 but none of the 5.0 specific features will be available. You would be using it as a eMMC 4.4/4.5. For this you would need to change the value of card->ext_csd.rev from 6 to 7. You may find more information on the thread below, it's not i.MX6UL specific but the logic would be the same.
i.mx6 with eMMC 5.0 SDR or DDR interface?
Regards,