iMX6SoloLite processor schematic/PCB symbol

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6SoloLite processor schematic/PCB symbol

跳至解决方案
1,509 次查看
Lankor
Contributor I

Can someone from Freescale convert the iMX6SL EVK schematic(SCH-27452_B.DSN) from OrCAD to Altium format? Or convert it into other format that Altium can import. When I tried to import the schematic, it showed "can't recognize the file".

Thanks too much!

标签 (1)
0 项奖励
1 解答
983 次查看
Yuri
NXP Employee
NXP Employee

Please try the enclosed (as result of saving as 16.2 version).

在原帖中查看解决方案

0 项奖励
4 回复数
984 次查看
Yuri
NXP Employee
NXP Employee

Please try the enclosed (as result of saving as 16.2 version).

0 项奖励
983 次查看
Lankor
Contributor I

Thank you, Yuri. I can import it into Altium now.

0 项奖励
983 次查看
raghavendraanja
Contributor II

Just install the cadence evaluation setup in the system where you have Altium and then import it works.

i have done the translation from .dsn to altium.

983 次查看
hippo
NXP TechSupport
NXP TechSupport

you can find an OrCAD DSN file saved at version 16.2

version after 16.2 are not supported on Altium. The original one is 16.3