iMX6Q/S CSI capture from FPGA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q/S CSI capture from FPGA

860 Views
jaroslaw_glazow
Contributor I

Hello all,
I have a question a little bit on a silly side. I have a FPGA unit which outputs pre-configured 1080@30 fps video (with typical parameters one can see in such signals), and I want to capture it with gstreamer (v4l2). I managed to capture this video on other vendor SOCs while working on other projects, but I have no clue how to capture it with IMX, my naive approach was to strip-down existing drivers (ov5640 or tc358743), but my lack of knowledge about driver development on iMX slows me down. Is there any simpler way?

Best regards,
Jarek 

Labels (2)
Tags (1)
0 Kudos
2 Replies

735 Views
zhouqi
Contributor II

Hi Jarek 

   sorry to interrupt you

    Have you solved this problem later?

    I get the same porblem now? Can you give me some suggestion or your solution way.

   Thank you very much .

Best regards

zhou

    

0 Kudos

761 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jarek 

one can look at Chapter 21 Configuring the Camera Preview Driver

sdk document included in "1.1.0_iMX6_Platform_SDK.zip" on

SMP Enable in IMX6 

Linux/Android tutorials:

Android Camera - Variscite Wiki 

Parallel camera | ConnectCore 6 

15. i.MX Video Capture Driver — The Linux Kernel documentation 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos