iMX6 solo problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6 solo problem

跳至解决方案
1,363 次查看
wanglee
Contributor III

My mfgtools support  iMX6Q/iMX6D,  it works right.  but it didn't  support my iMX6 solo. when the power on, "No Device Connected".  I don't think this is a hardware problem.  what should I DO?   CHANGE the settings  of mfgtool ?~ZFILHAZJN4K56YS[]95U}Q.png

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,198 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Please try using the recent MFG 

http://www.nxp.com/webapp/Download?colCode=IMX6_L4-1-15_2-0-0_MFG-TOOL&appType=license&location=null... 

 

  Also, please check if the i.MX6 S board is configured for serial (USB) boot mode ;

BOOT_MODE[1:0] = 01 (Serial Downloader).

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,199 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Please try using the recent MFG 

http://www.nxp.com/webapp/Download?colCode=IMX6_L4-1-15_2-0-0_MFG-TOOL&appType=license&location=null... 

 

  Also, please check if the i.MX6 S board is configured for serial (USB) boot mode ;

BOOT_MODE[1:0] = 01 (Serial Downloader).

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

 

0 项奖励
回复
1,198 次查看
wanglee
Contributor III

NOW ,the new tool (mfgtools-without-rootfs) can  find  my  iMX6Q .  when power on ,it shows HID-compliant device. then  START,  it always get stuck  in here  what is the problem?

9D$U{($FHK{}(U]N%J2HNC8.png

0 项奖励
回复
1,198 次查看
wanglee
Contributor III

The recent MFG, it works.  thanks.

0 项奖励
回复