iMX53 Copper Solder Pad & Soldermask size.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX53 Copper Solder Pad & Soldermask size.

796件の閲覧回数
T_I
Contributor I

We design our custom board based on MCIMX53-START-R.

I want to make the symbol of TEPBGA529 with Altium. But recommended PAD size is not found.

TEPBGA529 has 12mil PAD & 16mil Soldermask on MCIMX53-START-R. But I think that it is low reliability.

When I design BGA of 0.8mm, I always use the 14mil PAD and 18mil Soldermask.

I think that 16mil(0.4mm) pad is highest reliability, because solder balls of TEPBGA529 is 11.8mil(0.3mm) ~ 19.7mil(0.5mm).

how do you think?

102-TEPBGA.png

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

713件の閲覧回数
T_I
Contributor I

I overlooked it. I can do a design in peace.

Thanks,

0 件の賞賛
返信

713件の閲覧回数
ronak123
Contributor I

Go through MX53UG.pdf, 

Section 2.1 Basic Design Recommendations might be helpful.

Regards,

Ronak.

0 件の賞賛
返信