i.mx8mq with OV5640, one lane config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8mq with OV5640, one lane config

623 Views
subhasishghosh
Contributor II

Hi,

I am trying to configure OV5640 ( MINISASTOCSI) with the imx8mq EVM with one lane config. I followed the process as described in Single Lane Mipi interface to i.mx6 

However, the camera did not stream any data with the following command:

gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw,width=640,height=480 ! autovideosink

The same command works with the default 2 lane config.

I suspect the clock requirements on the DPHY side is not met.

Do we have any pointers on how to debug this for imx8. Most of the documentation available is for i.mx6 or 7.

I also changed the clock to as follows:

drivers/clk/imx/clk-imx8mq.c

clk_set_parent(clks[IMX8MQ_CLK_CSI2_CORE], clks[IMX8MQ_SYS1_PLL_800M]);

However, the camera still failed to stream.

Labels (1)
0 Kudos
1 Reply

535 Views
igorpadykov
NXP Employee
NXP Employee

Hi Subhasish

for one lane configuration one can look at

https://community.nxp.com/thread/498568 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos