i.MX8QM RPA_V17 request

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8QM RPA_V17 request

跳至解决方案
721 次查看
coindu
Contributor IV

Hi

           I want to use L4.19.35 bsp to compile i.MX8QM image. And  the ddr should be modify. So download SCFW source code about imx-scfw-porting-kit-1.2.7.1 , but when I download RPA , the older version is V20, but it will cause some compile error aboult RDBI_bit_deskew(0); function can not find.

 

         Can you send me the MX8QM_B0_LPDDR4_RPA_1.6GHz_v17.xlsx ?

0 项奖励
回复
1 解答
713 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hello coindu.

Please find attached file.

 

Best regards

Harvey

在原帖中查看解决方案

0 项奖励
回复
1 回复
714 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hello coindu.

Please find attached file.

 

Best regards

Harvey

0 项奖励
回复