i.MX8MQ: GIC v2 mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MQ: GIC v2 mode?

983 Views
bastian_schick
Contributor IV

Hi,

is the legacy mode (ARE == 0) fully supported?

So far, I get it working on a single core, but it seems the SGI/PPI registers exist only once for all core (instead being banked).

The chip errata does not list any issue regarding GIC.

Any tip is appreciated.

Labels (1)
Tags (4)
0 Kudos
2 Replies

786 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bastian

one can look at  codes gicv3_driver_init() which checks whether the GIC

supports the GICv2 compatibility mode

gicv3_main.c\v3\gic\arm\drivers - imx-atf - i.MX ARM Trusted firmware 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

786 Views
bastian_schick
Contributor IV

Did you read my question completely?

"is the legacy mode (ARE == 0) fully supported?

So far, I get it working on a single core, but it seems the SGI/PPI registers exist only once for all core (instead being banked).

The chip errata does not list any issue regarding GIC."

 

I can see that ARE is 0, so legacy mode should be supported. But in the CPU interface exists only once for all cores. Which is wrong. The registers for PPIs and SGIs should be banked. But they are _not_.

Therefore the question if I am just did not find the right address?

BTW: Why link and not just copy the relevant code?

0 Kudos