i.MX8MPlus Windows 10 IoT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MPlus Windows 10 IoT

ソリューションへジャンプ
2,011件の閲覧回数
leven
Contributor I

We use i.MX8MPlus to run Windows 10 IoT system and encounter the compatibility problem of Samsung eMMC. How to solve it? Details are as follows:

1. Failed to run Windows 10 IoT using Samsung /KLMAG1JETD-B041/16GB eMMC5.1

2. Windows 10 IoT was successfully run with Samsung /KLMAG2GEUF-B04P/16GB eMMC5.1.

3. The above two Samsung eMMC burning ubuntu system runs normally, but there is a difference in running Wingdows 10 IoT.

4. The picture shows the comparison between operation failure and success.Windows OK vs  NG.png

ラベル(1)
0 件の賞賛
返信
1 解決策
2,004件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There is no differences between eMMC it should works, just need erase and install the image, so far there is nothing report it.

 

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,938件の閲覧回数
anthonychen-msft
Contributor II

Do you have the datasheets for the two Samsung parts? I'm curious what their differences might be.

Also do you have the whole video showing where the script actually fails?

0 件の賞賛
返信
1,993件の閲覧回数
leven
Contributor I

Hi Bio_TICFSL:

We ran Windows 10 IoT with the new Samsung /KLMAG1JETD-B041/16GB chip and still failed.

We erased the Samsung /KLMAG1JETD-B041/16GB chip and still failed to run Windows 10 IoT.

Running the following command to erase also fails : 

# destroy the partition table

dd if=/dev/zero of=/dev/sdx bs=1024 count=1

0 件の賞賛
返信
1,594件の閲覧回数
mirkoardinghi1
Contributor IV

I have the same problem, Do you find a solution?

0 件の賞賛
返信
831件の閲覧回数
aber
Contributor III

By default, it only supports emmc above 32g. 

0 件の賞賛
返信
2,005件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There is no differences between eMMC it should works, just need erase and install the image, so far there is nothing report it.

 

Regards

0 件の賞賛
返信