i.MX8MPlus Windows 10 IoT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8MPlus Windows 10 IoT

跳至解决方案
2,137 次查看
leven
Contributor I

We use i.MX8MPlus to run Windows 10 IoT system and encounter the compatibility problem of Samsung eMMC. How to solve it? Details are as follows:

1. Failed to run Windows 10 IoT using Samsung /KLMAG1JETD-B041/16GB eMMC5.1

2. Windows 10 IoT was successfully run with Samsung /KLMAG2GEUF-B04P/16GB eMMC5.1.

3. The above two Samsung eMMC burning ubuntu system runs normally, but there is a difference in running Wingdows 10 IoT.

4. The picture shows the comparison between operation failure and success.Windows OK vs  NG.png

标签 (1)
0 项奖励
回复
1 解答
2,130 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There is no differences between eMMC it should works, just need erase and install the image, so far there is nothing report it.

 

Regards

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,064 次查看
anthonychen-msft
Contributor II

Do you have the datasheets for the two Samsung parts? I'm curious what their differences might be.

Also do you have the whole video showing where the script actually fails?

0 项奖励
回复
2,119 次查看
leven
Contributor I

Hi Bio_TICFSL:

We ran Windows 10 IoT with the new Samsung /KLMAG1JETD-B041/16GB chip and still failed.

We erased the Samsung /KLMAG1JETD-B041/16GB chip and still failed to run Windows 10 IoT.

Running the following command to erase also fails : 

# destroy the partition table

dd if=/dev/zero of=/dev/sdx bs=1024 count=1

0 项奖励
回复
1,720 次查看
mirkoardinghi1
Contributor IV

I have the same problem, Do you find a solution?

0 项奖励
回复
957 次查看
aber
Contributor III

By default, it only supports emmc above 32g. 

0 项奖励
回复
2,131 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There is no differences between eMMC it should works, just need erase and install the image, so far there is nothing report it.

 

Regards

0 项奖励
回复