i.MX8M mini M4 Core clock change

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M mini M4 Core clock change

ソリューションへジャンプ
1,026件の閲覧回数
m_morimune
Contributor I

Is there any problem with the i.MX8M mini when the M4 Core side changes the Core clock with its own program after startup?

For example, suppose that the CORE clock is raised to 400MHz with the following function of NXP_SDK after startup. 

 CLOCK_SetRootDivider (kCLOCK_RootM4, 1U, 2U);

 CLOCK_SetRootMux (kCLOCK_RootM4, kCLOCK_M4RootmuxSysPll1); / * switch cortex-m4 to SYSTEM PLL1 * /

In this case, can the clock be switched safely without causing glitches?

0 件の賞賛
返信
1 解決策
886件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Masahiro,

From the functionality point of view, no glitches should occur when switching clock modes (with the proper functions that waits for the lock of the PLLs).

However, if the SDK uses macros (on compile time) to generate the time bases (most of this, for FreeRTOS), the time bases may be broken when changing the clock bases on-on-the-fly. So, it is recommended applying the proper macro modification considering the clocks that are going to be used on the application and recompiling the SDK also including your custom functions for clock changes.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
887件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Masahiro,

From the functionality point of view, no glitches should occur when switching clock modes (with the proper functions that waits for the lock of the PLLs).

However, if the SDK uses macros (on compile time) to generate the time bases (most of this, for FreeRTOS), the time bases may be broken when changing the clock bases on-on-the-fly. So, it is recommended applying the proper macro modification considering the clocks that are going to be used on the application and recompiling the SDK also including your custom functions for clock changes.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信
886件の閲覧回数
m_morimune
Contributor I

Hi Carlos,

Thank you for your response.
I understood that there was no functional problem.
Also, thank you for contacting me about the cautions.

Best regards

masahiro

0 件の賞賛
返信