i.MX8 support for gstreamer-imx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 support for gstreamer-imx

Jump to solution
2,540 Views
yamazaki
Contributor II

I am trying to use gstreamer with i.MX8mmevk.
When I created yocto image and tried to add gstreamer-imx, the following error occurred and the build failed.

Parsing recipes: 100% |##########################################| Time: 0:05:04
Parsing of 2562 .bb files complete (0 cached, 2562 parsed). 3483 targets, 223 skipped, 8 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'gstreamer1.0-plugins-imx' (but /data/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/dynamic-layers/qt5-layer/recipes-fsl/images/fsl-image-qt5-validation-imx.bb RDEPENDS on or otherwise requires it)
gstreamer1.0-plugins-imx was skipped: incompatible with machine imx8mmevk (not in COMPATIBLE_MACHINE)
NOTE: Runtime target 'gstreamer1.0-plugins-imx' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['gstreamer1.0-plugins-imx']
ERROR: Required build target 'fsl-image-qt5-validation-imx' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-qt5-validation-imx', 'gstreamer1.0-plugins-imx']

So I realize can't build using gstreamer-imx with i.MX8mmevk.

Is there a way to use gstreamer-imx with i.MX8mmevk ?

Also, when will gstreamer1.0-plugins-imx_git.bb be compatible with i.MX8 ?

0 Kudos
1 Solution
2,134 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tadaharu

>when will gstreamer1.0-plugins-imx_git.bb be compatible with i.MX8 ?

gstreamer-imx is community version of plugins, which is not supported by nxp.

Suggestions for gstreamer-imx may be posted on gstreamer-imx github page

Issues · Freescale/gstreamer-imx · GitHub 

NXP supports imx-gst1.0-plugins from Code Aurora git repositories 

described in official linux documentation on link

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
2,135 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tadaharu

>when will gstreamer1.0-plugins-imx_git.bb be compatible with i.MX8 ?

gstreamer-imx is community version of plugins, which is not supported by nxp.

Suggestions for gstreamer-imx may be posted on gstreamer-imx github page

Issues · Freescale/gstreamer-imx · GitHub 

NXP supports imx-gst1.0-plugins from Code Aurora git repositories 

described in official linux documentation on link

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
2,134 Views
yamazaki
Contributor II

Hi, igorpadykov-san.

Sorry.

I certainly understood that it was not what I heard in NXP community.
Again, I will post on gstreamer-imx github page.

I look forward to answering another question.

0 Kudos
2,134 Views
yamazaki
Contributor II

Hi, igorpadykov-san.

 

Sorry.

The other is not the same as you hear here, too.

Thank you for answering.

0 Kudos