i.MX8 board hang on watchdog time out

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 board hang on watchdog time out

1,125 Views
amit_gondaliya
Contributor I

i.MX8 board hang on watchdog time out.

I have custom i.MX8 board ,

When I write below command on board, it got hanged and I need to do power cycle to make it functional again.

command

echo 1 > /dev/watchdog.

[Kernel configuration: imx2+ and imx8 watchdog driver are enable from kernel configuration.]

0 Kudos
1 Reply

971 Views
igorpadykov
NXP Employee
NXP Employee

Hi Amit

to have reliable wdog reset it is necessary to implement schematic

solution in such way, that this signal behaved as RESET SWITCH,

shortly removing all power supplies from board. For example

on i.MX8QM board SCU_WDOG_OUT i.MX8QM connected to

U23A, U10A (PC33PF8100) PMIC_WDOG_IN and acts as
"RESET SWITCH".

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos