i.MX6ULL NVCC_CSI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL NVCC_CSI

483 Views
sugiyamatoshihi
Contributor V

Hi,

If CSI doesn't use, is it possible to open NVCC_CSI pin?

Best Regards,

Sugiyama

Labels (1)
0 Kudos
2 Replies

372 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sugiyama

recommendations for unused module connections are given in

sect.3.2 Recommended Connections for Unused Analog Interfaces i.MX6ULL Datasheet
https://www.nxp.com/docs/en/data-sheet/IMX6ULLCEC.pdf

All other power supplies should be applied even its modules are not used

to avoid leakage from powered domains to unpowered.

So if CSI doesn't use, NVCC_CSI  power should be applied.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

372 Views
sugiyamatoshihi
Contributor V

Hi, Igor,

Thank you for answer.

I understood.

Best Regards,

Sugiyama

0 Kudos