i.MX6SDL eSPI BIT_COUNT and BURST_LENGTH.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SDL eSPI BIT_COUNT and BURST_LENGTH.

Jump to solution
620 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6S eCSPI BIT_COUND and BUSRT_LENGTH.

Please see the questions as below.

[Q1]

"BIT_COUNT" is mentioned in "21.7.3 Transmit Data Register (ECSPIx_TXDATA)" of reference manual (IMX6SDLRM Rev.1).

But, we can not find the bit field in "21.7.4 Control Register (ECSPIx_CONREG)" of reference manual.

I think "BIT_COUNT" is a misprint, "BURST_LENGTH" is correct, right?

[Q2]

Description of "BURST_LENGTH" is up to "2^7 words" written in "21.7.4 Control Register (ECSPIx_CONREG) Bit31:20" of reference manual.

We think this description shows "128 words", but we think there are only 64 words in FIFO.

Can you tell us relation of "BURST_LENGTH" and FIFO ?

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
1 Solution
460 Views
Yuri
NXP Employee
NXP Employee

Please look at my comments below.

1.

  Yes, it is assumed, that the BIT_COUNT is BURST_LENGTH.

2.
  FIFO size is less than the BURST_LENGTH : a transaction is not considered as
finished (SS is asserted) while all bits, defined via the field BURST_LENGTH, are
not transferred – with waiting (if needed) TXFIFO filling dynamically (during transfer).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
461 Views
Yuri
NXP Employee
NXP Employee

Please look at my comments below.

1.

  Yes, it is assumed, that the BIT_COUNT is BURST_LENGTH.

2.
  FIFO size is less than the BURST_LENGTH : a transaction is not considered as
finished (SS is asserted) while all bits, defined via the field BURST_LENGTH, are
not transferred – with waiting (if needed) TXFIFO filling dynamically (during transfer).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos