Hi,
I'm searching for the input specifications for CLK1_P,CLK1_N,CLK2_P&CLK2_N pins of i.MX6QP.
I couldn't find them in the datasheet. I also checked i.MX community as following.
https://community.nxp.com/message/360020
https://community.nxp.com/thread/446350
Does anyone know those value such as VIH, VIL and Tolerance?
Is it LVDS clock level compatible?
Can somebody help me to get them?
Solved! Go to Solution.
Hello,
According to Hardware Development Guide for i.MX6 in Table 2-7 (Oscillator
and clock recommendations:
"CLK1_P/CLK1_N and CLK2_P/CLK2_N are LVDS input/output differential pairs compatible with
TIA/EIA-644 standard. The frequency range is 0 to 600 MHz.
Alternatively, a single-ended signal can be used to drive a CLKx_P input. In this case, the corresponding
CLKx_N input should be tied to a constant voltage level equal to 50% of VDD_HIGH_CAP. Termination
should be provided with high-frequency signals. See the LVDS pad electrical specification in the data
sheet for further details."
http://cache.nxp.com/assets/documents/data/en/user-guides/IMX6DQ6SDLHDG.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
According to Hardware Development Guide for i.MX6 in Table 2-7 (Oscillator
and clock recommendations:
"CLK1_P/CLK1_N and CLK2_P/CLK2_N are LVDS input/output differential pairs compatible with
TIA/EIA-644 standard. The frequency range is 0 to 600 MHz.
Alternatively, a single-ended signal can be used to drive a CLKx_P input. In this case, the corresponding
CLKx_N input should be tied to a constant voltage level equal to 50% of VDD_HIGH_CAP. Termination
should be provided with high-frequency signals. See the LVDS pad electrical specification in the data
sheet for further details."
http://cache.nxp.com/assets/documents/data/en/user-guides/IMX6DQ6SDLHDG.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------