i.MX6Q SABRE-AI GPIO control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q SABRE-AI GPIO control

1,458 Views
waynelou
Contributor I

Hello everyone,

I am working on imx6q sabre-AI board on Android 7.1 with Linux4.1.15. Now I am porting TI wl18xx wifi SDIO module to usdhc2 SD slot. But I cannot control the GPIO pin as wifi enable pin to enable/disable the wifi module.

Below is my dts configuration about wifi and usdhc:

wlan_en_reg: fixedregulator@2 {
compatible = "regulator-fixed";
regulator-name = "wlan-en-regulator";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;

/* WLAN_EN GPIO for this board – Bank2, pin7 */
gpio = <&gpio2 7 GPIO_ACTIVE_HIGH>; //MX6QDL_PAD_NANDF_D7__GPIO2_IO07 --> WL_REG_ON/WL_EN

/* WLAN card specific delay */
startup-delay-us = <70000>;
enable-active-high;
regulator-boot-on;
};

&usdhc2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc2_wifi>;
bus-width = <4>;
// no-1-8-v; //justin@20170606 Mornco target board will remove this
wifi-host;
pm-ignore-notify;
keep-power-in-suspend;
enable-sdio-wakeup;
//ty:1234
vmmc-supply = <&reg_3p3v>;
vqmmc-supply = <&wlan_en_reg>;
//ocr-limit = <0x80>;
#power-off-card;
#no-1-8-v;
non-removable;
enable-sdio-wakeup;
status = "okay";

 wlcore: wlcore@0 {
         pinctrl-names = "default";
         compatible = "ti,wl1835";
         reg = <2>;
         interrupt-parent = <&gpio2>;
         interrupts = <5 IRQ_TYPE_EDGE_RISING>; //MX6QDL_PAD_NANDF_D5__GPIO2_IO05 --> WL_IRQ
       // platform-quirks = <1>;
         board-ref-clock = <4>; /* BOARD reference clock, See /include/linux/wl12xx.h for more info*/

};
};

pinctrl_usdhc2_wifi: usdhc2wifigrp {
fsl,pins = <
MX6QDL_PAD_SD2_CMD__SD2_CMD 0x17069
MX6QDL_PAD_SD2_CLK__SD2_CLK 0x10069
MX6QDL_PAD_SD2_DAT0__SD2_DATA0 0x17069
MX6QDL_PAD_SD2_DAT1__SD2_DATA1 0x17069
MX6QDL_PAD_SD2_DAT2__SD2_DATA2 0x17069
MX6QDL_PAD_SD2_DAT3__SD2_DATA3 0x17069
MX6QDL_PAD_NANDF_D5__GPIO2_IO05 0x17069 //0x13059 // this is for WL_IRQ which driver will configure as an input with a pull down
MX6QDL_PAD_NANDF_D7__GPIO2_IO07 0x13059 // WL_REG_ON/WL_EN
>;
};

But when I connected GPIO2_IO07(wlan_en pin) to the module, I can't control that pin by using

ifconfig wlan0 up & ifconfig wlan0 down

When I probe that pin, it always at high once boot up the board and never goes to low. That pin is located in J32, #26pins

1.png

I can't even control this pin using sysfs entry as GPIO by below way:

echo 39 > /sys/class/gpio/export

echo out > /sys/class/gpio/gpio39/direction

echo 1 > /sys/class/gpio/gpio39/value

echo 0 > /sys/class/gpio/gpio39/value

It always remain high(3.3V) and never goes to low when I echo 0 to the value.

Can anyone help me how to control the high/low of this pin as GPIO in J32?

BR,

Wayne

Labels (2)
0 Kudos
6 Replies

1,152 Views
waynelou
Contributor I

Thanks all.

I have solved this issue by doing right configuration in DTS.

BR,

Wayne

0 Kudos

1,152 Views
jerseyyang
Contributor III

what is  the root cause?  regulator-boot-on or wrong pad?

0 Kudos

1,152 Views
waynelou
Contributor I

Hi Jersey,

Just use:

vmmc-supply = <&wlan_en_reg>; no "vqmmc-supply".

BR,

Wayne

0 Kudos

1,152 Views
BrianW
Contributor I

Glad you got it working.  I am working on similar stuff, can you post full dtb or patch file so I can see it?

0 Kudos

1,152 Views
jerseyyang
Contributor III

Hi Wayne Lou:

           1. you need check whether the GPIO2_IO07's iomux's PAD is correct or not, if it is correct, it seems the DTS

pin configuation is no problem.

            2. with echo command to drive GPIO2_IO07, then try to more test point with this Pin, not just Pin 26 of J32, also R210's end close to U25's DATA7. it seems R210 not installed in your demo board according to the schematic.

            3. if possible, you can directly test the pad of Pin GPIO2_IO07 near to the CPU. until to the point of Pin26.

frankly speaking, i encounter the similar issue, which there is lack of a resister installed in the demo board. it always keeps low,  i check the line step by step close to CPU, and found the root cause. good luck to you.

0 Kudos

1,152 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wayne

please check gpio iomux settings with jtag or with printf,

try to toggle it with jtag to check if this is not hardware issue.

For usage GPIO sysfs entry one can look at

Definitive GPIO guide - Studio Kousagi Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos