i.MX6DQ QuadSPI boot.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6DQ QuadSPI boot.

跳至解决方案
857 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ.

Please see chapter 8.6 in IMX6DQRM Rev.2, it say i.MX6DQ can QuadSPI boot.

However, there is no description about QuadSPI other than this chapter.

And according to Quad SPI availability with iMX6, i.MX6 cannot use QuadSPI.

Is chapter 8.6 misprint? or i.MX6DQ was updated to use QuadSPI?

If i.MX6DQ can use QuadSPI boot, could you let me know the connection and IOMUX setting also?

Best Regards,

Satoshi Shimoda

标签 (2)
标记 (1)
0 项奖励
1 解答
646 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi,

sorry i.MX6DQ can not use QuadSPI boot,

IMX6DQRM Rev.2 has misprint (this material is from next IMX6SLXRM).

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
1 回复
647 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi,

sorry i.MX6DQ can not use QuadSPI boot,

IMX6DQRM Rev.2 has misprint (this material is from next IMX6SLXRM).

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励