Hi All,
I was writing PCI driver on the SabreSD to communicate with Altera FPGA over PCI.
I think I have damaged the PCI port on the chip after unplugging and plugging the FPGA board again. I was very careful to power down both boards before plugging / unplugging but looks like that is not enough.
Now I still can boot the SabreSD board connect UART console and SSH to it but the PCI is not working. I tried a reference PCI Network card and it’s not working.
I tried to investigate the problem and this is my findings:
imx6q-pcie 1ffc000.pcie: phy link never came up
imx6q-pcie 1ffc000.pcie: Failed to bring link up!
imx6q-pcie 1ffc000.pcie: failed to initialize host
imx6q-pcie: probe of 1ffc000.pcie failed with error -22
# cat /proc/cpu/alignment
User: 0
System: 7
Skipped: 0
Half: 0
Word: 0
DWord: 0
Multi: 7
User faults: 2 (fixup)
root@imx6qsabresd:/sys/devices/system/cpu#
root@imx6qsabresd:/sys/devices/system/cpu# cat /proc/cpuinfo
processor : 0
model name : ARMv7 Processor rev 10 (v7l)
BogoMIPS : 3.00
Features : swp half thumb fastmult vfp edsp neon vfpv3 tls vfpd32
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc09
CPU revision : 10
processor : 1
model name : ARMv7 Processor rev 10 (v7l)
BogoMIPS : 3.00
Features : swp half thumb fastmult vfp edsp neon vfpv3 tls vfpd32
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc09
CPU revision : 10
Hardware : Freescale i.MX6 Quad/DualLite (Device Tree)
Revision : 0000
Serial : 0000000000000000
Is it possible that I have accidentally disabled the clock “clock gate” some blocks in the Chip? How do I enable it again?
root@imx6qsabresd:/unit_tests# ./dump-clocks.sh
clock parent flags en_cnt pre_cnt rate
ckil --- 00000030 0 0 32768
ckih1 --- 00000030 0 0 0
osc --- 00000030 6 6 24000000
pll1_bypass_src osc 000002a2 1 1 24000000
pll1 pll1_bypass_src 00000041 1 1 996000000
pll1_bypass pll1 000002a6 1 1 996000000
pll1_sys pll1_bypass 00000024 1 1 996000000
pll1_sw pll1_sys 000002a0 1 1 996000000
arm pll1_sw 00000004 2 2 996000000
twd arm 00000024 1 1 498000000
pll2_bypass_src osc 000002a2 1 1 24000000
pll2 pll2_bypass_src 00000041 1 1 528000000
pll2_bypass pll2 000002a6 1 1 528000000
pll2_bus pll2_bypass 00000024 2 2 528000000
pll2_pfd0_352m pll2_bus 00000000 0 0 452571428
ldb_di0_sel pll2_pfd0_352m 000002a4 0 0 452571428
ldb_di0_div_3_5 ldb_di0_sel 00000024 0 0 129306122
ldb_di0_div_7 ldb_di0_sel 00000024 0 0 64653061
ldb_di0_div_sel ldb_di0_div_7 000002a6 0 0 64653061
ldb_di0 ldb_di0_div_sel 00000005 0 0 64653061
ldb_di1_sel pll2_pfd0_352m 000002a4 0 0 452571428
ldb_di1_div_3_5 ldb_di1_sel 00000024 0 0 129306122
ldb_di1_div_7 ldb_di1_sel 00000024 0 0 64653061
ldb_di1_div_sel ldb_di1_div_7 000002a6 0 0 64653061
ldb_di1 ldb_di1_div_sel 00000005 0 0 64653061
ipu2_di1_sel ldb_di1 000002a6 0 0 64653061
ipu2_di1 ipu2_di1_sel 00000005 0 0 64653061
ipu2_pclk1_sel ipu2_di1 00000000 0 0 64653061
ipu2_pclk1_div ipu2_pclk1_sel 00000004 0 0 64653061
ipu2_pclk_1 ipu2_pclk1_div 00000004 0 0 64653061
pll2_pfd1_594m pll2_bus 00000000 0 0 594000000
gpu3d_shader_sel pll2_pfd1_594m 000002a2 0 0 594000000
gpu3d_shader gpu3d_shader_sel 00000025 0 0 594000000
pll2_pfd2_396m pll2_bus 00000000 1 1 396000000
pll2_198m pll2_pfd2_396m 00000024 0 0 198000000
step pll2_pfd2_396m 000002a2 0 0 396000000
hsi_tx_sel pll2_pfd2_396m 000002a2 1 1 396000000
hsi_tx_podf hsi_tx_sel 00000025 1 1 198000000
hsi_tx hsi_tx_podf 00000005 1 1 198000000
usdhc1_sel pll2_pfd2_396m 00000000 0 0 396000000
usdhc1_podf usdhc1_sel 00000025 0 0 198000000
usdhc1 usdhc1_podf 00000005 0 0 198000000
usdhc2_sel pll2_pfd2_396m 00000000 0 0 396000000
usdhc2_podf usdhc2_sel 00000025 0 0 198000000
usdhc2 usdhc2_podf 00000005 0 0 198000000
usdhc3_sel pll2_pfd2_396m 00000000 0 0 396000000
usdhc3_podf usdhc3_sel 00000025 0 0 198000000
usdhc3 usdhc3_podf 00000005 0 0 198000000
gpmi_apb usdhc3 00000005 0 0 198000000
gpmi_bch_apb usdhc3 00000005 0 0 198000000
per1_bch usdhc3 00000005 0 0 198000000
apbh_dma usdhc3 00000005 0 0 198000000
usdhc4_sel pll2_pfd2_396m 00000000 0 0 396000000
usdhc4_podf usdhc4_sel 00000025 0 0 198000000
usdhc4 usdhc4_podf 00000005 0 0 198000000
gpmi_bch usdhc4 00000005 0 0 198000000
emi_sel pll2_pfd2_396m 00000000 0 0 396000000
emi_podf emi_sel 00000004 0 0 198000000
enfc_sel pll2_pfd2_396m 000002a2 0 0 396000000
enfc_pred enfc_sel 00000025 0 0 79200000
enfc_podf enfc_pred 00000025 0 0 19800000
enfc enfc_podf 00000005 0 0 19800000
gpmi_io enfc 00000005 0 0 19800000
periph_pre pll2_bus 000002a0 1 1 528000000
periph periph_pre 00000080 2 2 528000000
ahb periph 00000004 8 8 132000000
ipg ahb 00000025 4 4 66000000
ipg_per ipg 00000004 0 0 66000000
gpt_ipg_per ipg_per 00000005 0 0 66000000
i2c1 ipg_per 00000005 0 0 66000000
i2c2 ipg_per 00000005 0 0 66000000
i2c3 ipg_per 00000005 0 0 66000000
pwm1 ipg_per 00000005 0 0 66000000
pwm2 ipg_per 00000005 0 0 66000000
pwm3 ipg_per 00000005 0 0 66000000
pwm4 ipg_per 00000005 0 0 66000000
caam_ipg ipg 00000005 1 1 66000000
can1_ipg ipg 00000005 0 0 66000000
can2_ipg ipg 00000005 0 0 66000000
enet ipg 00000005 2 2 66000000
gpt_ipg ipg 00000005 1 1 66000000
iim ipg 00000005 0 0 66000000
spba ipg 00000005 0 0 66000000
spdif_gclk ipg 00000005 0 0 66000000
ssi1_ipg ipg 00000005 0 0 66000000
ssi2_ipg ipg 00000005 0 0 66000000
ssi3_ipg ipg 00000005 0 0 66000000
uart_ipg ipg 00000005 1 1 66000000
usboh3 ipg 00000005 0 0 66000000
cko1_sel ahb 000002a2 0 0 132000000
cko1_podf cko1_sel 00000025 0 0 16500000
cko1 cko1_podf 00000024 0 0 16500000
asrc_ipg ahb 00000005 0 0 132000000
asrc_mem ahb 00000005 0 0 132000000
caam_mem ahb 00000005 1 1 132000000
caam_aclk ahb 00000005 1 1 132000000
esai_ipg ahb 00000005 0 0 132000000
esai_mem ahb 00000005 0 0 132000000
hdmi_iahb ahb 00000005 1 1 132000000
ocram ahb 00000004 2 2 132000000
rom ahb 00000005 1 1 132000000
sata ahb 00000005 1 1 132000000
sdma ahb 00000005 8 8 132000000
mmdc_ch0_axi periph 00000004 1 1 528000000
ipu1_sel mmdc_ch0_axi 000002a2 0 0 528000000
ipu1_podf ipu1_sel 00000025 0 0 264000000
dcic1 ipu1_podf 00000005 0 0 264000000
ipu1 ipu1_podf 00000005 0 0 264000000
ipu1_pclk0_sel ipu1 00000000 0 0 264000000
ipu1_pclk0_div ipu1_pclk0_sel 00000004 0 0 0
ipu1_pclk_0 ipu1_pclk0_div 00000004 0 0 0
ipu1_pclk1_sel ipu1 00000000 0 0 264000000
ipu1_pclk1_div ipu1_pclk1_sel 00000004 0 0 0
ipu1_pclk_1 ipu1_pclk1_div 00000004 0 0 0
ipu2_sel mmdc_ch0_axi 000002a2 0 0 528000000
ipu2_podf ipu2_sel 00000025 0 0 264000000
dcic2 ipu2_podf 00000005 0 0 264000000
ipu2 ipu2_podf 00000005 0 0 264000000
ipu2_pclk0_sel ipu2 00000000 0 0 264000000
ipu2_pclk0_div ipu2_pclk0_sel 00000004 0 0 0
ipu2_pclk_0 ipu2_pclk0_div 00000004 0 0 0
gpu3d_core_sel mmdc_ch0_axi 000002a2 0 0 528000000
gpu3d_core_podf gpu3d_core_sel 00000025 0 0 528000000
gpu3d_core gpu3d_core_podf 00000005 0 0 528000000
periph2_pre pll2_bus 000002a2 0 0 528000000
periph2 periph2_pre 00000080 0 0 528000000
mmdc_ch1_axi periph2 00000004 0 0 528000000
pll3_bypass_src osc 000002a2 1 1 24000000
pll3 pll3_bypass_src 00000041 1 1 480000000
pll3_bypass pll3 000002a6 1 1 480000000
pll3_usb_otg pll3_bypass 00000024 3 3 480000000
usbphy1 pll3_usb_otg 00000024 0 0 480000000
pll3_pfd0_720m pll3_usb_otg 00000000 0 0 720000000
pll3_pfd1_540m pll3_usb_otg 00000000 2 2 540000000
video_27m pll3_pfd1_540m 00000024 0 0 27000000
hdmi_isfr pll3_pfd1_540m 00000005 1 1 540000000
axi_alt_sel pll3_pfd1_540m 000002a2 1 1 540000000
axi_sel axi_alt_sel 000002a0 1 1 540000000
axi axi_sel 00000004 2 2 270000000
gpu2d_axi axi 000002a2 0 0 270000000
gpu3d_axi axi 000002a2 0 0 270000000
pcie_axi_sel axi 000002a2 0 0 270000000
pcie_axi pcie_axi_sel 00000005 0 0 270000000
emi_slow_sel axi 00000000 1 1 270000000
emi_slow_podf emi_slow_sel 00000004 1 1 135000000
eim_slow emi_slow_podf 00000005 2 2 135000000
vdo_axi_sel axi 000002a2 0 0 270000000
vdo_axi vdo_axi_sel 00000005 0 0 270000000
vdoa vdo_axi 00000005 0 0 270000000
vpu_axi_sel axi 000002a2 0 0 270000000
vpu_axi_podf vpu_axi_sel 00000025 0 0 270000000
vpu_axi vpu_axi_podf 00000005 0 0 270000000
mlb axi 00000005 0 0 270000000
openvg_axi axi 00000005 0 0 270000000
pll3_pfd2_508m pll3_usb_otg 00000000 0 0 508235294
ssi1_sel pll3_pfd2_508m 00000000 0 0 508235294
ssi1_pred ssi1_sel 00000025 0 0 127058823
ssi1_podf ssi1_pred 00000025 0 0 63529411
ssi1 ssi1_podf 00000005 0 0 63529411
ssi2_sel pll3_pfd2_508m 00000000 0 0 508235294
ssi2_pred ssi2_sel 00000025 0 0 127058823
ssi2_podf ssi2_pred 00000025 0 0 63529411
ssi2 ssi2_podf 00000005 0 0 63529411
ssi3_sel pll3_pfd2_508m 00000000 0 0 508235294
ssi3_pred ssi3_sel 00000025 0 0 127058823
ssi3_podf ssi3_pred 00000025 0 0 63529411
ssi3 ssi3_podf 00000005 0 0 63529411
pll3_pfd3_454m pll3_usb_otg 00000000 0 0 454736842
spdif_sel pll3_pfd3_454m 000002a2 0 0 454736842
spdif_pred spdif_sel 00000025 0 0 227368421
spdif_podf spdif_pred 00000025 0 0 28421052
spdif spdif_podf 00000005 0 0 28421052
pll3_120m pll3_usb_otg 00000024 0 0 120000000
pll3_80m pll3_usb_otg 00000024 1 1 80000000
uart_serial_podf pll3_80m 00000025 1 1 80000000
uart_serial uart_serial_podf 00000005 1 1 80000000
pll3_60m pll3_usb_otg 00000024 0 0 60000000
ecspi_root pll3_60m 00000025 0 0 60000000
ecspi1 ecspi_root 00000005 0 0 60000000
ecspi2 ecspi_root 00000005 0 0 60000000
ecspi3 ecspi_root 00000005 0 0 60000000
ecspi4 ecspi_root 00000005 0 0 60000000
ecspi5 ecspi_root 00000005 0 0 60000000
can_root pll3_60m 00000025 0 0 30000000
can1_serial can_root 00000005 0 0 30000000
can2_serial can_root 00000005 0 0 30000000
periph_clk2_sel pll3_usb_otg 000002a0 0 0 480000000
periph_clk2 periph_clk2_sel 00000025 0 0 480000000
periph2_clk2_sel pll3_usb_otg 000002a2 0 0 480000000
periph2_clk2 periph2_clk2_sel 00000025 0 0 480000000
esai_sel pll3_usb_otg 000002a2 0 0 480000000
esai_pred esai_sel 00000025 0 0 240000000
esai_podf esai_pred 00000025 0 0 30000000
esai_extal esai_podf 00000005 0 0 30000000
asrc_sel pll3_usb_otg 000002a2 0 0 480000000
asrc_pred asrc_sel 00000025 0 0 240000000
asrc_podf asrc_pred 00000025 0 0 30000000
asrc asrc_podf 00000005 0 0 30000000
gpu2d_core_sel pll3_usb_otg 000002a2 0 0 480000000
gpu2d_core_podf gpu2d_core_sel 00000025 0 0 480000000
gpu2d_core gpu2d_core_podf 00000005 0 0 480000000
pll4_bypass_src osc 000002a2 0 0 24000000
pll4 pll4_bypass_src 00000041 0 0 147456000
pll4_bypass pll4 000002a6 0 0 147456000
pll4_audio pll4_bypass 00000024 0 0 147456000
pll4_post_div pll4_audio 00000025 0 0 36864000
pll4_audio_div pll4_post_div 00000025 0 0 36864000
pll5_bypass_src osc 000002a2 0 0 24000000
pll5 pll5_bypass_src 00000041 0 0 296600000
pll5_bypass pll5 000002a6 0 0 296600000
pll5_video pll5_bypass 00000024 0 0 296600000
pll5_post_div pll5_video 00000025 0 0 74150000
pll5_video_div pll5_post_div 00000025 0 0 74150000
ipu1_di0_pre_sel pll5_video_div 000002a6 0 0 74150000
ipu1_di0_pre ipu1_di0_pre_sel 00000025 0 0 24716666
ipu1_di0_sel ipu1_di0_pre 000002a6 0 0 24716666
ipu1_di0 ipu1_di0_sel 00000005 0 0 24716666
ipu1_di1_pre_sel pll5_video_div 000002a6 0 0 74150000
ipu1_di1_pre ipu1_di1_pre_sel 00000025 0 0 24716666
ipu1_di1_sel ipu1_di1_pre 000002a6 0 0 24716666
ipu1_di1 ipu1_di1_sel 00000005 0 0 24716666
ipu2_di0_pre_sel pll5_video_div 000002a6 0 0 74150000
ipu2_di0_pre ipu2_di0_pre_sel 00000025 0 0 24716666
ipu2_di0_sel ipu2_di0_pre 000002a6 0 0 24716666
ipu2_di0 ipu2_di0_sel 00000005 0 0 24716666
ipu2_di1_pre_sel pll5_video_div 000002a6 0 0 74150000
ipu2_di1_pre ipu2_di1_pre_sel 00000025 0 0 24716666
pll6_bypass_src osc 000002a2 1 1 24000000
pll6 pll6_bypass_src 00000041 1 1 500000000
pll6_bypass pll6 000002a6 1 1 500000000
pll6_enet pll6_bypass 00000024 1 1 500000000
sata_ref pll6_enet 00000024 0 0 100000000
sata_ref_100m sata_ref 00000024 0 0 100000000
lvds1_sel sata_ref 000002a2 0 0 100000000
lvds1_gate lvds1_sel 00000004 0 0 100000000
pcie_ref pll6_enet 00000024 0 0 125000000
pcie_ref_125m pcie_ref 00000024 0 0 125000000
enet_ref pll6_enet 00000020 1 1 125000000
pll7_bypass_src osc 000002a2 1 1 24000000
pll7 pll7_bypass_src 00000041 1 1 480000000
pll7_bypass pll7 000002a6 1 1 480000000
pll7_usb_host pll7_bypass 00000024 1 1 480000000
usbphy2 pll7_usb_host 00000024 1 1 480000000
gpt_3m osc 00000024 1 1 3000000
cko2_sel osc 000002a2 0 0 24000000
cko2_podf cko2_sel 00000025 0 0 24000000
cko2 cko2_podf 00000024 0 0 24000000
cko cko2 000002a2 0 0 24000000
dummy --- 00000030 2 2 0
usbphy1_gate dummy 00000024 1 1 0
usbphy2_gate dummy 00000024 1 1 0
lvds2_sel dummy 000002a2 0 0 0
lvds2_gate lvds2_sel 00000004 0 0 0
anaclk1 --- 00000030 0 0 0
lvds1_in anaclk1 00000004 0 0 0
anaclk2 --- 00000030 0 0 0
lvds2_in anaclk2 00000004 0 0 0
orphans --- 00000004 0 0 0
root@imx6qsabresd:/unit_tests#
Hi Tarek
it may be useful to look at following resources how to check PCIe signals :
"PCIe Certification Guide for i.MX 6 :"
http://cache.freescale.com/files/32bit/doc/app_note/AN4784.pdf
"QA: About i.Mx6 PCIe compliance"
https://community.freescale.com/docs/DOC-95554
"How to setup i.MX6Dual/Quad and i.MX6Solo/DualLite Linux software for PCIe compliance Test?"
https://community.freescale.com/docs/DOC-94923
and try attached bare-metal sdk pcie test.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for the information. All the documents you have provided is talking about compliance test. what I need is to bring back the PCI link to life.
I have tested the bare-metal sdk pcie test but that did not work. I get error message: Link timeout ! when running the test.
What could be the problem?
Thanks
Hi Igor,
I have tried a reference Ethernet card 100% sure that it's working in a PC and currently not working with the SabreSD board. The same card use to work before with the Sabre board.
I'm not sure about the RST_B and the signal timing. I am using The Freescale reference board and Freescale reference Linux software.
How do I modify the signals and the timing?
Also I would expect the HW/SW to be configure to accommodate most PCI cards in the market or do I need to keep changing the configuration for each card?
Is there any Power-Gating registers for PCI that I need to check?
Thanks,
Tarek
Hi Igor,
Let me clarify this. I have 2 SabreSD boards running the same software. On one board PCI is working fine while the other it stopped working recently. I've tried the same PCI-NIC card and the Same SD card on both boards one is working and one is not.
The faulty board is not sending the training sequence at initialization as I can see on the oscilloscope and the PCI analyzer. The IOMUXC_GPR8 will adjust the amplitude and de-emphasis of the TX signal. But if there is no signal this is not going to help!
As I mentioned before I have tested a version of bare-metal SDK and I get Link timeout ! when running the PCI test.
Is there any point from running the attached file you provided? I'm not sure how to compile it on it's own. Do you have some instructions?
Thanks,
Tarek
Hi Tarek
NXP has a service which process a return of failure board.
Best regards
igor