i.MX6 SSI and AUDMUX

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX6 SSI and AUDMUX

Jump to solution
1,196 Views
宗標廖
Contributor V

Hello,Community

According to IMX6DQRM, there are only 3 SSI interfaces on i.MX6D/Q processor,but now I want to connect 4 audio devices to i.MX6,what should I do?

Thank you!

ZongbiaoLiao

pastedImage_0.png

0 Kudos
1 Solution
371 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi ZongbiaoLiao

one can use network mode, example is described in AN2628

Figure 10 Connecting to Two External Devices in SSI Network Mode

http://cache.freescale.com/files/32bit/doc/app_note/AN2628.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
7 Replies
371 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi ZongbiaoLiao

  default BSP(L3.0.35_4.1.0) does not support this

suggest to look at sect.16.5.1.1.2 Internal Network Mode

http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf

Best regards

igor

0 Kudos
372 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi ZongbiaoLiao

one can use network mode, example is described in AN2628

Figure 10 Connecting to Two External Devices in SSI Network Mode

http://cache.freescale.com/files/32bit/doc/app_note/AN2628.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
371 Views
宗標廖
Contributor V

Hi igor

Thank you for your reply,it's helpful!

I have one more question as bellow.

I want to use AUDMUX external port as bellow(take port4 as example),is this implementation right?

Audio device1 uses Tx function of port4 and Audio device2 uses Rx function of port4. And I want device1 and device2 work simultaneously.

pastedImage_0.png

0 Kudos
371 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi ZongbiaoLiao

yes it is right.

~igor

0 Kudos
371 Views
宗標廖
Contributor V

Hi igor

Please give me a reply!

0 Kudos
371 Views
宗標廖
Contributor V

Hi igor

Could you give me an answer?

Thank you very much!

0 Kudos
371 Views
宗標廖
Contributor V

Hi, igor

Thank you for your reply!

I am sorry for having some more questions!

Q1):

For the implementation as above, should SSI1 be master or slave?

And does the default BSP(L3.0.35_4.1.0) support this?

Q2):

According to AN2628, I think i.MX6 supports the following mode.

Does it need to connect a pull-up resistor on both AUD3_TXD and AUD4_TXD? And how to decide the resistance?

Thank you!

pastedImage_1.png

0 Kudos