i.MX6 SATA PHY. RTerm calibration resistor!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 SATA PHY. RTerm calibration resistor!

Jump to solution
1,935 Views
martinchristian
Contributor II

How to determine the value of (ResRef) RTerm calibration resistor on the SATA PHY?

On the "iMX6 Smart device system" the value is 191R 1%, why?

Labels (1)
0 Kudos
1 Solution
1,252 Views
martinchristian
Contributor II

Hi,

The closest I have come to a description of the resistor value, is found here:

Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors.

IMX6DQ6SDLHDG, Rev 1, 06/2013

Section 2.2 table 2-13

"SATA_REXT – Connect an external 191 Ω 1% resistor to GND."

"The impedance calibration process requires connection of this reference resistor.

If SATA is unused, the reference resistor may be populated if desired for manufacturability purposes, or left no-connect for cost savings."

/Martin.

View solution in original post

0 Kudos
4 Replies
1,253 Views
martinchristian
Contributor II

Hi,

The closest I have come to a description of the resistor value, is found here:

Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors.

IMX6DQ6SDLHDG, Rev 1, 06/2013

Section 2.2 table 2-13

"SATA_REXT – Connect an external 191 Ω 1% resistor to GND."

"The impedance calibration process requires connection of this reference resistor.

If SATA is unused, the reference resistor may be populated if desired for manufacturability purposes, or left no-connect for cost savings."

/Martin.

0 Kudos
1,252 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

from MX6DQ sect.54.1.4 Block Descriptions :

"RTerm Tuning -This block uses an external resistor (ResRef) as reference to

determine the proper calibration setting for centering the Rx and Tx termination

resistances at 50 ohms."

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,252 Views
martinchristian
Contributor II

Chip,

Yes this is correct, I also found this description in the Reference manual.
But nothing about what the value of the resistor should be... That is my question..

0 Kudos
1,252 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

value you can find in i.MX6 SDP/SDB schematic

"MX6_SABRE_SDP_DESIGNFILES "

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&fpsp=1&tab=Design_Too...

Best regards

chip