i.MX6 Quad 4G bytes DDR stress test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Quad 4G bytes DDR stress test

Jump to solution
848 Views
m_c
Senior Contributor I

Is it right to choose "9" when DDR stress test ask select DDR density per chip select for 4G bytes?

pastedImage_0.png

Labels (1)
Tags (2)
0 Kudos
1 Solution
548 Views
Yuri
NXP Employee
NXP Employee

   Yes, it is right to choose "9".


Have a great day,
Yuri
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
549 Views
Yuri
NXP Employee
NXP Employee

   Yes, it is right to choose "9".


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos