i.MX53 VPU status monitor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 VPU status monitor

Jump to solution
562 Views
torus1000
Contributor V

Hi,

I think it would be worth when decoder appication debug to know which frame now processed.

Is there any such status bit information for i.MX53 VPU(C&M Coda754x)?

If someone knows this, please let me know. I couldn't find it.

Labels (2)
Tags (2)
0 Kudos
1 Solution
482 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I am afraid there is no such debug info, just because

video encoding is quite complex algorithm, depending on many factors.

Available API are provided in document i.MX5x_Linux_VPU_API.pdf included in

IMX53_1109_LINUXDOCS_BUNDLE

Best regards

igor
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
483 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I am afraid there is no such debug info, just because

video encoding is quite complex algorithm, depending on many factors.

Available API are provided in document i.MX5x_Linux_VPU_API.pdf included in

IMX53_1109_LINUXDOCS_BUNDLE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos