i.MX51 LVDS color and 2.6.38 [solved]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX51 LVDS color and 2.6.38 [solved]

618 Views
GiuseppePagano
Contributor I

Hi all,

I'm working on a custom i.MX51 babbage board.

When I migrated from kernel 2.6.35 to freescale git branch  imx_2.6.38_11.11.01 (and also imx_2.6.38_11.09.01 and imx_2.6.38) we noticed that the six low significative bit of blue color (from DISP1_D0 to DISP1_D5) was no more active.

The effect is that blu have a "gross" definition; red and green are ok: 8 bit color depth each oen.

If we rollback to 2-6-35 all return pk. 

We sow the same  behavior on an original Freescale i.MX51 Babbage. Does anyone notice this problem too ? Any idea to solve ?

We are using video default configuration, (we also try other but nothing changed: kernel 2.6.35 works, 2.6.38 doesn't)

    .interface_pix_fmt = IPU_PIX_FMT_RGB24,
    .mode_str = "1024x768M-16@60",
    .default_bpp = 16,

we tested both dvi and LVDS output.

Hope someone can help me, just to say if his or her babbage board wors ok with 2.6.38

Bye

Giuseppe

Tags (1)
0 Kudos
1 Reply

501 Views
GiuseppePagano
Contributor I

I solved. Write here the solution for future reference.

In this moment on Freescale GIT repository they miss this piece of code from file:

   "arch/arm/mach-mx5/cpu.c":

#include <linux/clk.h>
#include <linux/err.h>

........................

static void __init ipu_mipi_setup(void)
{
struct clk *hsc_clk;
void __iomem *hsc_addr;

hsc_addr = MX51_IO_ADDRESS(MX51_MIPI_HSC_BASE_ADDR);

hsc_clk = clk_get_sys(NULL, "mipi_hsp");
if (IS_ERR(hsc_clk)) {
pr_err("failed to get mipi clock\n");
return;
}
clk_enable(hsc_clk);

/* setup MIPI module to legacy mode */
__raw_writel(0xf00, hsc_addr);

/* CSI mode: reserved; DI control mode: legacy (from Freescale BSP) */
__raw_writel(__raw_readl(hsc_addr + 0x800) | 0x30ff,
hsc_addr + 0x800);

clk_disable(hsc_clk);
clk_put(hsc_clk);
}

static int __init post_cpu_init(void)
{
unsigned int reg;
void __iomem *base;

if (cpu_is_mx51())
ipu_mipi_setup();

..................

Bye

Giuseppe

0 Kudos