i.MX50: How to use USBH1_PWR pin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX50: How to use USBH1_PWR pin?

Jump to solution
715 Views
norishinozaki
Contributor V

Hello Champs,

I'd like to use a USBH1_PWR pin to control an PMIC to feed power for USB devices.

I found a register to change the polarity(H1_PWR_POL) in USBOH1_USB_CTRL register, however which register I can use toggle the pin?

From RM, SW_MUX_CTL_PAD_EPITO (IOMUXC_SMUXC_PEPITO)

001 Select mux mode: ALT1 mux port: GPIO[27] of instance: gpio6.

010 Select mux mode: ALT2 mux port: USBH1_PWR of instance: usboh1.

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
1 Solution
647 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
2 Replies
648 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
647 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

this signal should be controlled by PP bit in PORTSC register.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos