i.MX 8M Mini: about M4 wake up A53 through RPMsg

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Mini: about M4 wake up A53 through RPMsg

2,899 Views
yanghui
Contributor I

Hi all:

I want to wake up the sleeping A53 with M4 via RPMsg,  but I found it failed . I need your help.

 

  I did an experiment with reference to the following post. Where is the RPMsg document for IMX8MM? 

  The result is successful implementation of RPMsg communication.

pastedImage_3.png

 

Based on the above experiments, I modified the experiment:

The practice is :

1. modify the firmware of M4 (rpmsg_lite_str_echo_rtos_imxcm4.bin). When M4 receives the RPMsg sent by A53, it will    delay 10s, then reply A53 message.

2. In this 10s process, if the command below is executed on the control terminal of A53:

      echo mem > /sys/power/state     [CMD 1]

At this time, A53 is not woken up, and M4 does not send an RPMsg reply message.

 

During the 10s process, if the command below is executed on the control terminal of A53:

     

 echo freeze > /sys/power/state   [CMD 2]

At this time, A53 is not woken up, and M4 can send an RPMsg reply message.

 

So my question is how to make M4 wake up A53 through RPMsg when A53 enters sleep mode via command([CMD 1] or [CMD 2]).

 

Thank you for your help.

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

1,909 Views
siva_prabhakara
Contributor III

did u figure it out, how to do this?

0 Kudos
Reply

1,909 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You could take a look at the low-power suggestions from application note AN12195, available on the following link:

https://www.nxp.com/docs/en/application-note/AN12195.pdf

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply

1,366 Views
DavidC1
Contributor II

I'm having a similar problem.  I have an RPMSG communication channel between the A53 and M4 cores on an i.MX8 mini.

If I put Linux to sleep, it seems to put the M4 to sleep as well (its background processing stops), so the code running there can't send an RPMSG packet, which should in theory wake the A53.

I downloaded application note AN12195, but it doesn't seem to have links to the test application or the Linux driver patches needed to make it work.  The document refers to several patch files, but doesn't seem to have any links I can follow in order to get those files.

Can someone here provide necessary links so I can get my M4 software to wake the A53?

0 Kudos
Reply

1,352 Views
DavidC1
Contributor II

I was able to find the code for AN1215.  Unfortunately, it is meant for an imx8mq SoC.

I tried porting the kernel changes over to the imx8mm, but it doesn't work.  With that change, my M4 doesn't run at all.

Is there an application note somewhere to show how to do this (sleep the A53 while not sleeping the M4) on an imx8mm SoC?

0 Kudos
Reply