Hi Xianbao
usb speed is detected automatically during enumeration (state of D+/D- lines), for details one can refer to
usb2.0 specification or simple description on
https://www.beyondlogic.org/usbnutshell/usb2.shtml
Best regards
igor
Hi Igor
I know usb speed is detected automatically during enumeration (state of D+/D- lines).
I see in the IMX8 datasheet(USBx_nPORTSC1 register bit of PFSC ) and the Chipidea /core.c:654 driver file that the configuration port is supported only at full speed connection.But,I don't see information in the IMX8 USB register instructions about configuring only low speed connections.
Does USB OTG support driver configuration to connect only at low speeds?
Best regards
xianbao
>Does USB OTG support driver configuration to connect only at low speeds?
I am afraid not, sorry.
Best regards
igor
Thank you very much for your answer,Maybe I made a mistake.
On other platforms, USB speed can be limited by the “maximum-speed” attribute of the USB device tree node, but no configuration logic for USB speed is found in the IMX8USBOTG driver. Can I limit the USB speed to low-speed through the driver? If so, how to configure it?
Best regards
xianbao