i.MX 8M Mini Evaluation Kit Max WiFi Connections

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Mini Evaluation Kit Max WiFi Connections

764 Views
jpagnotta
Contributor I

We are working with the i.MX 8M Mini Evaluation Kit to prototype a new system.  Currently, it appears as though the maximum number of simultaneous WiFi connections is limited to five. The DHCP is properly configured to lease out more than five addresses.  

Is this limit controlled by the processor or selected wireless chip used on the eval kit?  Can this be modified?

Labels (1)
Tags (1)
0 Kudos
3 Replies

591 Views
radhikasomaiya
Senior Contributor II

Hi Jason Pagnotta,

Let us know which bsp version and OS you are using?

Regards,

Radhika Somaiya.

0 Kudos

591 Views
jpagnotta
Contributor I

Thanks for responding radhika.somaiya@volansystech.com.  We are using i.MX Linux Yocto Project BSP 4.14.98_2.0.0 Release, Linux Kernel 4.14.98.

0 Kudos

591 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,Jason Pagnotta,

>>CPU & BSP

CPU and linux don't limit ti.

>> WIFI chipset & wifi driver

WIFI chipset and WIFI driver don't limit.

>> WIFI firmware

For most WIFI module, firmware limit the number of client to access the AP.

>> try to modify it.

You can try to change hostapd.conf file, which is  probably feasible. But if it has been limited in firmware, the way will be invalid.

>>About other WIFI modules

I asked some WIFI providers or manufactures, such as realtek, and broadcomm, their max numbers for AP clients is 8 or 10.

So I advise you to modify hostapd.conf file to adjust the number.

Have a nice day!

BR,

Weidong

0 Kudos