i.MX 6UL: how to use HAB API

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 6UL: how to use HAB API

1,644 次查看
memrekaraaslan
Contributor II

Hello again Yuri

As you said, I read the documents https://www.nxp.com/docs/en/application-note/AN12263.pdf and High Assurance Boot Version 4 Application Programming Interface Reference Manual. I want to extend chain of trust and I guess, I should to use HAB API's. But I couldn't find any examples of them. For example, where should I use the Authenticate Image API function to validate the u-boot image? spl.c or hab.c or u-boot source code? I don't understand where to use the authentication APIs.

Thank you !

0 项奖励
回复
5 回复数

1,564 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent some comments directly.

Regards,

Yuri.

0 项奖励
回复

1,419 次查看
matthoe
Contributor I

Hi Yuri,

I am also working on High Assurance Boot (for i.MX6ULL) and try to extend the chain of trust by authenicating addiditonal images, e.g. the kernel. For me it is also unclear how to use the HAB API. Do you have additional information and examples? Thanks!

best regards

0 项奖励
回复

1,407 次查看
Yuri
NXP Employee
NXP Employee
0 项奖励
回复

1,564 次查看
TonyYan
Contributor I

Hi Yuri,

I am also working on the HAB, could you send me the example as well?

thanks.

Tony

0 项奖励
回复

1,564 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  As I see Victor    picked up Your request. He will answer soon. 
I also will check it.

Regards,

Yuri.

0 项奖励
回复