how to interface wifi module (453-00045C ) to mimxrt117x- evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to interface wifi module (453-00045C ) to mimxrt117x- evk

383件の閲覧回数
akash-lawande
Contributor II

Hello, I trying to integrate wifi module (453-00045C) from laird  with EVK kit using SDIO protocol from sdk  2.12.0 wifi cli example but not able to get any signal 

so hardware connected wifi module to  EVK

SDIO_CLK------>U19G.D15 (mimxrt117x- evk processor)

SDIO_CMD----->U19G.B16 (mimxrt117x- evk processor)

SDIO_D0------->U19G.C15 (mimxrt117x- evk processor) 

SDIO_D1------->U19G.B17 (mimxrt117x- evk processor)

SDIO_D2------->U19G.B15 (mimxrt117x- evk processor)

SDIO_D3------->U19G.A16 (mimxrt117x- evk processor)

can anyone help on this ??    

0 件の賞賛
返信
1 返信

360件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @akash-lawande ,

 

Sorry for our delay reply!

Not sure if the issue has been resolved. 

I checked your connections of SDIO interface, it is no problem.

For communications between WiFi and MCU, please pay attention to IO Level on both sides. by default, on CPU side, SDIO IO Level is 3.3V. if you need 1.8V,  a jumper should be used on J55.

 

Regards,

weidong

0 件の賞賛
返信