how can i enable PPS on ENET2_EVENT0_OUT
02-27-2019
03:37 AM
1,509 次查看
2 回复数
03-12-2019
03:28 AM
1,382 次查看
Hi
thx for your reply. The PPS signal has been found.
yes, i use ptp4l. after setting "phc2sys -w -s /dev/ptp0 -d /dev/pps0 -m" and echo 1 > /sys/class/ptp/ptp0/pps_enable, the PPS has been found.
thanks a lot.
I have another question, if one imx6 act as GMC which can output PPS, another imx6 act as slave(OC) which also can PPS.
both of them run "ptp4l -i eth0 -2 -H -m" , after "locked", as the master offset is about [-100, 100] nS. if PPS of two board has the same phase position? or, Is the phase shift should less than microsecond?