Hi,
I'm using e-con Systems Camera ar1335_af with DART-MX8MQ via MIPI !
I'm using Yocto dunfell, and i apply this patch varigit/meta-econ-imx to my wayland yocto image due to the fact Varicite and NXP maintened the variwiki just for sumo fsl 4.14.98 yocto.
I sucess to compile the driver and apply all necessary patch for yocto dunfell !
But when i try to get picture or video from camera with :
gst-launch-1.0 v4l2src
the colorimetry of source are really weird, like you can see below :
to get picture i use the commande :
gst-launch-1.0 -e v4l2src device=/dev/video0 num-buffers=1 ! video/x-raw,width=1920,height=1080 ! jpegenc ! filesink location=/tmp/img7.jpg
to get videoi use the commande :
gst-launch-1.0 v4l2src device=/dev/video0 num-buffers=100 ! video/x-raw,width=1920,height=1080 ! jpegenc ! avimux ! filesink location=./test0.avi
I don't know where the problem could come from, linux command problem? clock frequency? mipi lanes?
Thanks for help !
Hello,
I guess the problem is bad connection of mipi lanes.
Regards
The connection of mipi lanes seem working !
The e-con Systems Camera ar1335_af support juste the YUYV video format, isn't that the reason the output id like that ! ?