gcc tool chain in i.mx7d sabre board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gcc tool chain in i.mx7d sabre board

1,995件の閲覧回数
dharmeshkanzari
Contributor II

Hello i am using i.mx7d sabre board and, os is Linux L4.1.15_1.2.0 GA.

When i am trying to compile c program but can't compile it. I want to use gcc is there any way to install gcc is 'Linux L4.1.15_1.2.0 GA'. Please help me.

 if there is already any other tool chain then help me how to use it, and hoe to compile c program in i.mx7.

Dharmesh.

ラベル(1)
3 返答(返信)

1,162件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

please refer to the following how to use the toolchain for NXP Linux BSP :

 

i.MX Yocto Project: How can I compile the kernel manually? 

https://community.nxp.com/thread/394804 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,162件の閲覧回数
jasonl
Contributor II

I think you are totally misunderstood the question. He is trying to ask how to get gcc built-in in the image instead of asking building a custom image. Please read through the question before answering.

0 件の賞賛
返信

1,162件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  hope the following helps.

https://community.nxp.com/message/853792 

Regards,

Yuri.