ethernet phy issue with qualcomm ar8035 on i.MX8M Nano board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ethernet phy issue with qualcomm ar8035 on i.MX8M Nano board

3,165 Views
betanapallisandeepraj
Contributor III

Hi,

I am working on i.MX8M nano board with ddr4. We changed the default phy from AR8031 to AR8035. 

I think linux driver for both phy is at803x.c is common. Now I am getting below error while making the ethernet interface up. 

root@imx8mnevk:~# ifconfig eth0 up
[ 41.388469] fec 30be0000.ethernet eth0: Unable to connect to phy
ifconfig: SIOCSIFFLAGS: No such device
root@imx8mnevk:~#

I could see 1 functional block, 1 chip select register as differences between AR8031 and AR8035. 

Please find the pictures attached. What are the changes required in kernel or uboot to make the ethernet interface up? Any suggestions would help a lot. 

 

Thank you

Sandeep Raj

0 Kudos
3 Replies

3,115 Views
betanapallisandeepraj
Contributor III

Hi Igor,

I tried to add node like in imx6dl-riotboard.dts in imx8mn.dtsi. my probe function is failing with error 'Unable to connect to phy'. But with same image I could see 8031 phy attached successfully in dmesg log in another board. This seems my node is not triggering the 8035, but my node is still triggering the 8031 in the driver, is it?  

0 Kudos

3,104 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos

3,146 Views
igorpadykov
NXP Employee
NXP Employee