egl extension EGL_KHR_fence_sync on IMX7ULP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

egl extension EGL_KHR_fence_sync on IMX7ULP

986件の閲覧回数
Nico_H
Contributor II

Hello,

does anyone see on the IMX7ULP other egl extensions than EGL_EXT_client_extensions or EGL_EXT_platform_base?

According to the i.MX Graphics User's Guide there should be others than these two.

Especially I want to use the EGL_KHR_fence_sync because the vsync on eglSwapBuffers does not work, even if I set eglSwapInterval to 1.

 

Best regards,

Nico

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

965件の閲覧回数
Nico_H
Contributor II

984件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Nico_H,

GL_OES_EGL_sync is only available on GLES 1.1, other GLES APIs will report it as non supported

EGL_KHR_fence_sync is supported.Just There is no reference at all for VG_KHR_EGL_sync.

Also eglSwapInterval is not supported on current versions

Regards

 

0 件の賞賛
返信