eMMC interface on I.mx257

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC interface on I.mx257

511 Views
maheshk
Contributor II

Hi all,

I wanted to interface eMMC on I.MX257 processor, can anyone please share the information fon doing this?. I also wants the processor should boot from eMMC.

Awaiting for the valuable suggestions.

Thanks in advance

Mahesh

0 Kudos
1 Reply

431 Views
art
NXP Employee
NXP Employee

The i.MX25 series processors have the Enhanced Secured Digital Host Controller

(eSDHC) interface modules that support the operation of SD/SDIO/MMC/eMMC

devices. For more information, please refer to the Chapter 23 of the i.MX25

Reference Manual Rev.2 document, available on the NXP web site:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

The system boot through the eSDHC interface (in other words, boot from an eMMC

device, connected to the eSDHC interface) is also supported. For more

information, refer to the Chapter 7  "System Boot" of the document above.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos