hi there :
1 how to run /power up can bus for A35 of I.MX8QXPC0 ?
2 M4 core is not use in current issure.
3 please give us some documents /guidelines/tips. thanks:
4 version: Embed linux kernel 5.10.9.1.0.0.
5 build project :yocto project. bitbake imx-image-full.
Hi Jack
for using flexcan on A35 it is necessary to use dts file without *rpmsg*:
&flexcan1 {
..
status = "okay"
If M4 is used, M4 flexcan resources has to be unassigned from M4 partition (board.c of SCFW), example
Best regards
igor
what did you mean with out "rpmsg"?
1 did you mean exclude all the dts dtsi named with fields "rpmsg" ?
thanks
>what did you mean with out "rpmsg"?
example with rpmsg : "imx8qxp-mek-dsi-rm67191-rpmsg.dts"
Best regards
igor