can imx6dl deal with 2 parallel cameras ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can imx6dl deal with 2 parallel cameras ?

390 Views
robingcao
Contributor I

Hi ,

At first we  use imx6q to deal with the two cameras,cause it has two IPUs.

Now I want to know if imx6dl can deal the two cameras too? 

I mean one through IPU, and the another one directly send data to DDR, Could this possible ? How

Labels (2)
0 Kudos
1 Reply

330 Views
Yuri
NXP Employee
NXP Employee

Hello,

   i.MX 6DualLite has single IPU, which in its turn has two CSI (parallel) ports CSI0, CSI1.

But because of multiplexing, CSI pins may conflict with other modules ; in particular -

with (parallel) display port. Please use Pin Mux Tools to get proper configuration.

i.MX 6 Series Software and Development Tool|NXP

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos