agl nxp 4.9.88-2.0.0 compile error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

agl nxp 4.9.88-2.0.0 compile error

2,150 Views
305824281
Contributor I

$bitbake agl-demo-platform

ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: QA Issue: psplash: Files/directories were installed but not shipped in any package:
/lib/systemd/system/psplash-network.service
/lib/systemd/system/psplash-basic.service
Please set FILES such that these items are packaged. Alternatively if they are unneeded, avoid installing them or delete them within do_install.
psplash: 2 installed and not shipped files. [installed-vs-shipped]
ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: Fatal QA errors found, failing task.
ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: Function failed: do_package
ERROR: Logfile of failure stored in: /home/zengguang/nxp_4.9.88/bld-agl/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/psplash/0.1+gitAUTOINC+2015f7073e-r15/temp/log.do_package.123587
ERROR: Task (/home/zengguang/nxp_4.9.88/sources/poky/meta/recipes-core/psplash/psplash_git.bb:do_package) failed with exit code '1'

0 Kudos
5 Replies

1,671 Views
vsuneja63
Contributor III

Hi Guang Zeng,

I am facing the same error when building AGL Master sources. if you have resolved this please share your solution.

0 Kudos

1,672 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Guang Zeng,

Are you following this guide?

https://source.codeaurora.org/external/imx/meta-nxp-agl/about/

If so, which version of Ubuntu are you using on your host? 16.04 is the recommended version as of today. I haven’t seen a similar error but I could try to reproduce it if you host is Ubuntu 16.04.

Regards,

0 Kudos

1,672 Views
305824281
Contributor I

hi gusarambula:

   I used ubuntu16.04

 

           

           I follow these step:

           1、I modify local.conf,because my app needs qt5.9 support.

              IMAGE_INSTALL_append = " qtbase qtbase-plugins qtwayland cinematicexperience liberation-fonts \
qtserialbus \
"
PACKAGECONFIG_FONTS_append_pn-qtbase = " fontconfig"

           2、 $: bitbake agl-image-minimal

            I download the image and ran the APP with an error after starting up.

            error:

            Failed to create display (No such file or directory)

        3、$: bitbake agl-image-weston

             compile error:

             ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: QA Issue: psplash: Files/directories were installed but not shipped in any package:
/lib/systemd/system/psplash-network.service
/lib/systemd/system/psplash-basic.service

         

        4、$: bitbake agl-demo-platform

              compile error,the error messeage is in the attachment

0 Kudos

1,672 Views
manizillion
Contributor IV

Hello Guang Zeng,

How did you solve this issue, iam also facing the same issue,  pls reply with solution  ... ???

ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: QA Issue: psplash: Files/directories were installed but not shipped in any package:
  /lib/systemd/system/psplash-basic.service
  /lib/systemd/system/psplash-network.service
Please set FILES such that these items are packaged. Alternatively if they are unneeded, avoid installing them or delete them within do_install.
psplash: 2 installed and not shipped files. [installed-vs-shipped]
ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: Fatal QA errors found, failing task.
ERROR: psplash-0.1+gitAUTOINC+2015f7073e-r15 do_package: Function failed: do_package
ERROR: Logfile of failure stored in: /home/imx8/weston-imx8/bld-agl/tmp/work/aarch64-poky-linux/psplash/0.1+gitAUTOINC+2015f7073e-r15/temp/log.do_package.23886
ERROR: Task (/home/imx8/weston-imx8/sources/poky/meta/recipes-core/psplash/psplash_git.bb:do_package) failed with exit code '1'

0 Kudos

1,672 Views
manizillion
Contributor IV

What is the solution to this issue ?

Regards

Mani

0 Kudos