WiFi Display Sink (Miracast) in i.MX8M Quad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WiFi Display Sink (Miracast) in i.MX8M Quad

683 Views
KojiTajima
Contributor II

Hello team,

I want to display the smartphone screen on the monitor of the HDMI output destination with miracast using the Linux environment running on i.MX8M Quad EVKB.

Looking at "https://community.nxp.com/t5/i-MX-Processors/WiFi-Display-Sink-Miracast-in-imx8QM/mp/1096870", it says that i.MX8QM does not support miracast. Does the i.MX8M Quad support miracast?

Is there any material such as the procedure to perform miracast and the command to use?

 

The environment I'm using : 

Linux imx8mqevk 5.10.52-lts-5.10.y+ga11753a89ec6 #1 SMP PREEMPT Wed Sep 8 10:41:11 UTC 2021 aarch64 aarch64 aarch64 GNU/Linux

 

Best regards,

KojiTajima

0 Kudos
3 Replies

621 Views
KojiTajima
Contributor II

Hi,

Do I absolutely need an optional Wi-Fi module like AW_CM358xxx to do miracast on i.MX8M Quad?

Is it possible to miracast in an environment where a Wi-Fi router is connected to the LAN port by wire even without a Wi-Fi module?

 

Best regards,

KojiTajima

0 Kudos

651 Views
KojiTajima
Contributor II

Hi, joanxie

Thank you for your reply. I will contact the Professional Services with the same content.

Thanks,

KojiTajima

0 Kudos

657 Views
joanxie
NXP TechSupport
NXP TechSupport

as I known, imx8mq can support this, for more detailed information, pls submit the case to the professional service as below:

"https://www.nxp.com/design/software/embedded-software/miracast-for-linux:MIRACAST-FOR-LINUX"

0 Kudos