Wi-Fi with uBlox ODIN-W160

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wi-Fi with uBlox ODIN-W160

951 Views
nanjundam
Contributor II

Hi,

I want to use wifi module uBlox ODIN-W160 with i.Mx6Q (MCIMX6Q6AVT10AD).

Does i.Mx6Q support this wifi module (ODIN-W160 ) ?

Please let me know anybody have tested ODIN-W160 for Wi-Fi interface over SDIO for i.Mx6Q.

 

Thanks & Regards,

Nanjunda M

ODIN-W160
Labels (3)
0 Kudos
Reply
2 Replies

655 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Regarding SDIO Wi-Fi cards, you could refer to the AR6103 SiP SD45 which is actually supported by several BSPs. You could also take as reference the following Community thread:

SABRE for Automotive Infotainment Modules


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

655 Views
nanjundam
Contributor II

Hi

Has anyone used this device with i.Mx6Q ?

Thanks & Regards,

Nanjunda M

0 Kudos
Reply