Why are some of the hardware/imx drivers tagged as 'eng'?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why are some of the hardware/imx drivers tagged as 'eng'?

888 Views
jaapdejong
Contributor I

I am using the android_M6_0.1_2.0.0_source drivers for our android board, and (for example) lights.imx6 does not get included on our user builds because it is tagged as 'eng' in LOCAL_MODULE_TAGS in hardware/imx/lights/Android.mk.

Why is this module tagged as 'eng'? It looks mature enough, any risks if I change the tag to optional?

Regards

Labels (1)
0 Kudos
Reply
1 Reply

805 Views
SergioSolis
NXP Employee
NXP Employee

Were you able to change it to opt?, you should be able to do it and not have a problem with it.

0 Kudos
Reply