Which version of the kernel uses DRM [imx6q-sabresd]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which version of the kernel uses DRM [imx6q-sabresd]

660 Views
ttttttx
Contributor III

I want to use the drm framework  to implement lvds display on imx6q-sabresd board. I tried L4.9.88 and found that there are many things that need to be changed. I visually inspected L4.19.35 and it seems to use FBDEV too.

So, which version of the Yocto  kernel  used  DRM?

0 Kudos
1 Reply

618 Views
art
NXP Employee
NXP Employee

The Direct Render Model (DRM) feature is not supported for the i.MX6 series processors. It is only supported for the i.MX8, i.MX8X and i.MX8M processor families starting from the 4.9.123 kernel.

Best Regards,
Artur

0 Kudos