Which SECO firmware version to be used with 5.15.52-2.1.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which SECO firmware version to be used with 5.15.52-2.1.0

Jump to solution
647 Views
philippe_schenk
Contributor IV

Hello

We're currently integrating the NXP Release LF5.15.52_2.1.0 for our products based on i.MX 8 (QM and QP) and i.MX 8QXP (and DX).

For that I integrated the per Release Notes recommended SCFW 1.14.0. In the release notes document of the SCFW it is written that the SECO is tested against the following versions:

5.8.7: i.MX8DXL-A1/i.MX8DXL-B0
3.8.5: i.MX8QM/i.MX8QXP
1.1.6: i.MX8DXL-A1-V2X/i.MX8DXL-B0-V2X

 

In the "i.MX Linux Release Notes" it is suggested to use `imx-seco-5.8.7.1.bin` for "i.MX 8QuadMax, 8QuadXPlus, and 8DXL reference boards".

Could you elaborate which version of SECO we should use for SoCs i.MX 8QuadMax, i.MX 8QuadPlus, i.MX 8QuadXPlus, i.MX 8DualX together with SCFW 1.14.0 on release LF5.15.52_2.1.0?

Thanks and Best Regards,
Philippe

0 Kudos
1 Solution
625 Views
philippe_schenk
Contributor IV

We figured it out in the meantime. The SHA256SUM of the SECO from 3.8.5/3.8.6 and 5.8.7.1 are the same for the SoCs mentioned in the original question.

View solution in original post

0 Kudos
1 Reply
626 Views
philippe_schenk
Contributor IV

We figured it out in the meantime. The SHA256SUM of the SECO from 3.8.5/3.8.6 and 5.8.7.1 are the same for the SoCs mentioned in the original question.

0 Kudos