Which MPU in i.MX family support ODT for DDR2 devices.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which MPU in i.MX family support ODT for DDR2 devices.

Jump to solution
876 Views
王剑翰
Contributor III

Do only I.MX51 and the above version i.MX MPU support the odt function for DDR2 devices?

Labels (5)
0 Kudos
1 Solution
743 Views
Yuri
NXP Employee
NXP Employee

  Basically the following devices support ODT for DDR2 :

i.MX28

i.MX50
i.MX51

i.MX53


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
744 Views
Yuri
NXP Employee
NXP Employee

  Basically the following devices support ODT for DDR2 :

i.MX28

i.MX50
i.MX51

i.MX53


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
743 Views
王剑翰
Contributor III

Hi Yuri,

I'm deeply grateful for all the trouble you've taken!

Thanks & BR

Jehan Wang

0 Kudos