Where I can download L5.1.1_2.1.0-HDCP2.x.tar.gz file?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where I can download L5.1.1_2.1.0-HDCP2.x.tar.gz file?

4,162 Views
ashleysheng
Contributor III

I'm working on HAB function on imx6q platform and the operating system is Android 5.1. I downloaded all documents associated to android 5.1.

According to one of the documents named AndroidTM HDCP2.x User's Guide Rev.L51.1_2.1.0-ga, 01/26, I need to download the L5.1.1_2.1.0-HDCP2.x.tar.gz file and then unpack it in order to get HDCPLib.tar.gz , xzvf mxc_secureboot.tar.gz and xzvf Patches.tar.gz . I searched NXP community, but I still can't find the file. Can anyone tell me where I can download L5.1.1_2.1.0-HDCP2.x.tar.gz Thanks.

Tags (1)
0 Kudos
Reply
13 Replies

3,795 Views
wilsonchen
Contributor III

你好,是否可以发一份L5.1.1_2.1.0-HDCP2.x.tar.gz呢,我公司这里也在研究这个。或者是否需要什么条件进行申请?

0 Kudos
Reply

3,795 Views
joanxie
NXP TechSupport
NXP TechSupport

这个是内部资料,如果你需要可以在官网提交问题,然后单独发给你

0 Kudos
Reply

3,795 Views
yenchao
Contributor IV

Hi Joan Xie,

I'm working on android 5.1 and also need L5.1.1_2.1.0-HDCP2.x.tar.gz package too.

Could you send me this package?

Or could you advise me where to apply this package.

Thx

Yen

0 Kudos
Reply

3,795 Views
joanxie
NXP TechSupport
NXP TechSupport

https://community.nxp.com/docs/DOC-329745

pls create a new thread to get it.

0 Kudos
Reply

3,795 Views
llliu
Contributor I

你好,我现在使用安卓7.1.2,需要一份mxc_secureboot.tar.gz的文件,来签名安卓的镜像文件。我在技术支持提交了申请后网页就再也进不去了。你可以单独发我一份文件吗?谢谢你了。

0 Kudos
Reply

3,795 Views
joanxie
NXP TechSupport
NXP TechSupport

unfortunately, we couldn't send to customer directly, pls try to submit a ticket again.

0 Kudos
Reply

3,795 Views
joanxie
NXP TechSupport
NXP TechSupport

pls find the attachment.

3,795 Views
wilsonchen
Contributor III

I also want to use the L5.1.1_2.1.0-HDCP2.x.tar.gz ,can you send me one?

0 Kudos
Reply

3,795 Views
ashleysheng
Contributor III

Hi ,

0 Kudos
Reply

3,795 Views
joanxie
NXP TechSupport
NXP TechSupport

Hi Ashley,

have your downloaded it already? if not, pls give me your mail address, I send it to you directly.

0 Kudos
Reply

3,795 Views
ashleysheng
Contributor III

Hi

0 Kudos
Reply

3,795 Views
Yuri
NXP Employee
NXP Employee

Hi !

is this package free ?

Regards,

Yuri.

0 Kudos
Reply

3,795 Views
joanxie
NXP TechSupport
NXP TechSupport

hi Yuri,

thanks for your reminder.

0 Kudos
Reply