What is the different for eFuse MAC_ADDR_LOCK (OP/WP)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the different for eFuse MAC_ADDR_LOCK (OP/WP)?

Jump to solution
719 Views
m_c
Senior Contributor I

As title.

pastedImage_1.png

Labels (2)
Tags (3)
0 Kudos
1 Solution
580 Views
Yuri
NXP Employee
NXP Employee

Hello,

Usually one may use the fuse override feature to test applications,
which read fuses, but not for boot. The override fuse values will be lost

upon reset, since the values are stored in registers.


Have a great day,
Yuri
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
581 Views
Yuri
NXP Employee
NXP Employee

Hello,

Usually one may use the fuse override feature to test applications,
which read fuses, but not for boot. The override fuse values will be lost

upon reset, since the values are stored in registers.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos