Voltage supply to i.MX6SL when DDR3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Voltage supply to i.MX6SL when DDR3

1,101件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I'm using i.MX6SL and PF0100 and have question about voltage supply when I use DDR3.

Can MMPF0100F4AEP supply both NVCC_1P2V and NVCC_DRAM ?

According to the EVK's schematic, NVCC_1P2V and NVCC_DRAM are supplied from different LDO.

NVCC_1P2V is VGEN1 and NVCC_DRAM is SW3A/B.

However, MMPF0100F4AEP has only one 1.5V output.

So I plan to supply both NVCC_1P2V and NVCC_DRAM from SW3A/B.

Do I need to supply voltage separately ?

Ko-hey

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

902件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

recommended to power it from separate clean LDO as it is used by

oscillator circuit as described in datasheet

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

902件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

Thank you for your reply.

So NXP recommend to add external LDO for supplying 1.5V to NVCC_1P2V.

Is it correct ?

Ko-hey

0 件の賞賛
返信

902件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

yes correct.

Best regards

igor

0 件の賞賛
返信

902件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

I understand that NXP recommend to supply voltage to NVCC_1P2V separately.

Let me confirm about supplying NVCC_1P2V again.

Does NVCC_1P2V have to supply voltage before POR_B is asserted ?

MMPF0100F4AEP has LDO that isn't programed such as VGEN2.

If I can supply voltage to NVCC_1P2V after POR_B is asserted, I want to use those LDOs.

I would rather not add a external LDO as much as possible.

So please advise me.

Ko-hey

0 件の賞賛
返信

902件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

I found following Community.

https://community.freescale.com/message/405181#comment-405181

As far as I checked the community, it have to be supplied voltage to NVCC_1P2V separately.

Thank you for your corporation.

Ko-hey

0 件の賞賛
返信